DIO#.INV

Description

Sets or gets the polarity of a bi-directional I/O when configured as a digital input (see DIO#.DIR).

Value Description
0 - Active high The digital input state is 1 when voltage is applied to the IO pin
1 - Active low The digital input state is 1 when voltage is removed from the IO pin

Examples

Usage

When DIO#.DIR = 0 (input) then the corresponding DIO#.INV can be set to change the polarity of the input signal.

Code

--> DIO1.DIR 0

With 24V on DIO1:

--> DIO1.INV 0 //Active high
--> DIO1.STATE
1
--> DIO1.INV 1 //Active low
--> DIO1.STATE
0

With 0V on DIO1:

--> DIO1.INV 0 //Active high
--> DIO1.STATE
0
--> DIO1.INV 1 //Active low
--> DIO1.STATE
1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO1.INV

368ah

02h

Unsigned8

-

-

Read/Write

No

DIO2.INV

368bh

02h

Unsigned8

-

-

Read/Write

No

DIO3.INV

368ch

02h

Unsigned8

-

-

Read/Write

No

DIO4.INV

368dh

02h

Unsigned8

-

-

Read/Write

No

DIO5.INV

368eh

02h

Unsigned8

-

-

Read/Write

No

DIO6.INV

368fh

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DIO1.INV

22100

5654

Unsigned8

Read/Write

-

DIO2.INV

22101

5655

Unsigned8

Read/Write

-

DIO3.INV

22102

5656

Unsigned8

Read/Write

-

DIO4.INV

22103

5657

Unsigned8

Read/Write

-

DIO5.INV

22104

5658

Unsigned8

Read/Write

-

DIO6.INV

22105

5659

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO1.INV

22100

Unsigned8

Read/Write

-

DIO2.INV

22101

Unsigned8

Read/Write

-

DIO3.INV

22102

Unsigned8

Read/Write

-

DIO4.INV

22103

Unsigned8

Read/Write

-

DIO5.INV

22104

Unsigned8

Read/Write

-

DIO6.INV

22105

Unsigned8

Read/Write

-